How can we help you today?

Why do I get the error "PLC reservation failed" when trying to upgrade the firmware of my PLC using the EcoStruxure Automation Device Maintenance tool?

Issue:
"PLC reservation failed" error message when upgrade the firmware of my PLC using the EcoStruxure Automation Device Maintenance tool


Product Line:
EcoStruxure Automation Device Maintenance


Resolution:
The error is generated when there is an existing programming connection to the PLC and you try to connect to the PLC using the EcoStruxure Automation Device Maintenance tool. to clear the error, disconnect from the PLC with Control Expert/Unity Pro
image2

Schneider Electric Egypt and North East Africa