Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How can you start and stop the ATS480 softstart from the keypad (VW3A1113 or VW3A1111)?

Customer wants to use the Run and Stop buttons on the keypad to start and stop the motor.

 

To enable this function go to Menu 3: Complete Settings, and then Menu 3.8: Command channel.

Then select the Cmd channel 1 (or Cmd channel 2 if using the Command Switching function) and set it to HMI.
480 HMI

 

The soft start will still require 24VDC to be present on the Stop input in order to be able to run.

 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: