How can we help you today?

Ecostruxure Process Expert 2021: Auxiliary Tasks are not supported on M580 HotStandby Systems

This document explains on below shown error which happens in Ecostruxure Process Expert 2021, when user is creating an Auxiliary Task in refinement of Control project.

Auxilary

Basically creation of auxiliary Tasks is not supported for M580 Hot standby Controllers. In Ecostruxure Process Expert 2021, by default the M580 standalone Controller is set in inside refinement of control project and if user has created a Aux0/Aux1 Tasks while saving the Control project, system will not give any error and will be successful.

But, when User performs Build All, then M580 Hotstandby Controller will be considered which was configured in Topology and thus the above error will appear which will not give proper information to User. Therefore User can check in the refinement of Control Expert whether Aux0/Aux1 Tasks were being created. If created remove them to successfully build your Project.

This document applies to all the versions of EPE.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
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
Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center