Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Schneider Electric have Bi-directional Power meter?

Yes, the following meters:

EasyLogic™ PM2000 Power Meters,

PowerLogic™ PM5000 Power Meters

PowerLogic™ PM8000 Power Quality Meters

PowerLogic ION9000

All have bi-directional energy measurement feature i.e it will give energy import/delivered and energy export/received. Positive real power P(+) flows from the power source to the load. Negative real power P(-) flows from the load to the power source.