Where can you find suggested lugs selection for the ATV480 Soft Starters?
Issue:
ATS480 Suggested Lugs
Product Line:
ATS480 with bus bars.
Environment:
ATS480C14Y thru ATS480M12Y only
Cause:
Products are shipped with flat bus bars they will need lugs to connect power and motor wiring.
Resolution:
You will not find any Lug suggestions in the ATS480 installation manuals, and the end customer is responsible for providing their own lugs.
On other hand, you can find some lugs reference we can use with ATS480 available in the IEC contactors and Starters catalog.
Example only from the Starters Catalog:
Released for: Schneider Electric Egypt and North East Africa
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
Help Center
Find support resources for all your needs, in one place.