Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to install and remove option card on ATV630 and ATV930 Drives.
Issue:
How do I install an extended IO extension or Communication card on Altivar Process Drive?

Product Line:
ATV930, ATV630

Environment:
All

Cause:
NA

Resolution:
There are 2 Slots (A and B) underneath Control Terminal Blocks.
Slot A is on the right and Slot B is on the left as you are facing the VFD.
Slot A ids only used for Communication cards.
Slot B is only used for IOP Extension modules.
Slide the option card straight into the slot until hear a click.

In order to remove the card, press or push on the tab (PUSH is written on the tab) on the option card and slide it out.