Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why ViewX Fails to launch after displaying the splash screen.

Common causes of ViewX failing to launch after the splash screen appears.

ViewX can fail to launch after installing or performing an upgrade etc... for several reasons. This page lists some of the common problems seen and some potential ways to fix the problem.

Possible Problems:

Anti-Virus.
ViewX is trying to launch however, something external is preventing it from starting. Often, this is caused by anti-virus software. Please work with your IT department to make sure suitable exclusions are configured for your anti-virus software to allow proper ViewX operation. https://community.se.com/t5/Geo-SCADA-Knowledge-Base/Anti-virus-Scan-Exclusions/ba-p/278735

ViewX not installed properly.
A repair or reinstall would fix this issue

Crystal Reports Driver.
Crystal Reports driver or runtime engine is not installed in ViewX. ViewX fails to login as it tries to run the Crystal Reports driver that isn't installed. This issue can be fixed by uninstalling Crystal Report runtime engine, also running the installer and remove Crystal Reports from the server. In case Crystal Reports is being used, run the installer, and install Crystal Reports runtime engine and the Crystal Reports driver on both ViewX client and server.

Crystal Reports DLL.

Even when Crystal Reports is not installed, some DLL files may remain and prevent ViewX from starting.

Search for:
SE.Scada.ViewX.CrystalReports.Plugin.dll
in:
C:\Program Files (x86)\Schneider Electric\ClearSCADA\Modules

If found, delete these DLL files to resolve the issue.


CefSharp Files.
This issue usually appears after upgrading or downgrading ViewX client. The splash screen appears but ViewX does not launch. ViewX is failing to start due to the wrong version of a file being on disk CefSharp files. Unfortunately, repair and reinstall would not resolve this issue.
A workaround to solve this issue as follows:
On a PC with the problem, please check the folders:
C:\Program Files (x86)\Schneider Electric\ClearSCADA
and
C:\Program Files (x86)\Schneider Electric\ClearSCADA\Modules
Files named "CefSharp” are only expected in the Modules folder. If these files are located in the ClearSCADA folder, then they can be deleted. Alternatively, shut down the server, delete those files, and then notice that ViewX will start running as expected.

Version mismatch between Geo SCADA Server and Virtual ViewX (VVX) Server.

If both components are installed on the same machine but are running different versions, ViewX will fail to launch. This typically happens when the Geo SCADA server is upgraded but the VVX server is not. To avoid this issue, always ensure that both the Geo SCADA server and the VVX server are running the same version.


Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: