Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I assign Freewheel Stop to a Logic Input on AT320 drive?
Issue:
Programming Freewheel stop assignment to a Digital Input on ATV320.

Product Line:
Altivar 320, ATV320

Environment:
All models and serial numbers

Cause:
None

Resolution:
Goto DRI- > CONF > FULL > FUN- > STT- nSt and assign a logic input (LIx) as desired.
The stop is activated when the input changes to 0.
If the input returns to state 1 and the run command is still active, the motor will only restart if [2/3 wire control] (tCC) is set to [2 wire] (2C) and if [2 wire type] (tCt) is set to [Level] (LEL) or [Fwd priority] (PFO).
If not, a new run command must be sent.
Note: This function cannot be used with certain other functions. Follow the instructions in the Programming manual.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center