Watch our short video to understand how to use the rotary cam switches configurator:
Cam switch configurator is a tool used to configure rotary/cam switches. The configurator allows the user to specify the desired specifications and characteristics of the cam switch, such as the number of poles and contacts, the type of actuator, and the mounting style. The configurator then generates a unique code that can be used to order the switch with the specified specifications. #schneider #rotaryswitch #camswitch Advantages * Ensure that the customer orders the correct switch for their specific application. * Help customers easily specify the desired specifications and see how they will affect the switch’s performance * Help to save time and reduce the risk of ordering a switch that is not suitable for the application.
Cam switch configurator is a tool used to configure rotary/cam switches. The configurator allows the user to specify the desired specifications and characteristics of the cam switch, such as the number of poles and contacts, the type of actuator, and the mounting style. The configurator then generates a unique code that can be used to order the switch with the specified specifications. #schneider #rotaryswitch #camswitch Advantages * Ensure that the customer orders the correct switch for their specific application. * Help customers easily specify the desired specifications and see how they will affect the switch’s performance * Help to save time and reduce the risk of ordering a switch that is not suitable for the application.
Released for: Schneider Electric Egypt and North East Africa