Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When was each firmware version of ION8650 first shipped?
Issue
Want to know when a specific version of ION8650 firmware was released

Product
ION8650

Resolution
The table below has details on when each version of firmware was released. Note that not all versions of firmware are available anymore
Table of firmware release dates
FW Date
V004.040.001 January 1 2021
V004.031.002 August 7 2019
V004.031.001 April 23 2019
V004.031.000 November 16 2018
V004.030.000 May 17 2018
V004.021.002 November 7 2017
V004.021.000 April 24 2017
V004.020.001 March 06 2015
V409 February 18 2015
V408 November 10 2014
V407 July 25 2014
V406 March 25 2014
V405 August 12 2013
V404 April 4 2013
V403 March 7 2012
V402 June 15 2011