Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I generate a document with details of the NOC module configuration with an M580?
Right-click the desired module or device in the DTM Browser and select Print Device:
image
If this optional function is supported by a DTM, this function displays the device documentation (including configuration settings) in the PC’s default Internet browser, which can then be printed.

NOTE: Device information can be printed:
  • For only one device DTM at a time when that DTM is not open for editing in the Device Editor
  • Only when the DTM is disconnected from the physical device