Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
EcoStruxure Control Expert - What are the READ_STS_MX Limitations?
Product line
EcoStruxure Control Expert

Description
The block READ_STS_MX has the same limitations as the READ_VAR because it uses TCP/IP, when you use a READ_VAR you have to manage execution to your EF managing the reports, depending on the CPUs type or connection point EFs numbers in // can change.

image

Then you can use add an unlimited number of blocks to logic, but you must execute them sequentially or not exceed the number of simultaneous connections.

Here is a short example: How to know the absence of x80 IO in local M580 rack when it is configured as Device DDT ?

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center