Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why event ID in TS event buffer could have number 16 ?

1.   Issue :

Why event ID in TS event buffer could have number 16 ?

2.   Product Line :

BMXERT1604T ,BMXCRA31210, BMECRA31210

3.   Environment

All supported Windows OS

4.   Resolution
Event with ID 16 (SOE_UNCERTAIN ) is used to indicate that some events may be lost in the next sequence of events and user needs to check the why the TS buffer of BMXERT1604T (or BMxCRA31210) reaches full state.



Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: