How can we help you today?

Is there an isolated relay output card for the x80 I/O?

Yes the BMXDRA0815 is a 16 point isolated relay card.

BMXDRA0815 - discrete output module, Modicon X80, 8 NO relay outputs, 24 to 240V AC, 24 to 125V DC | Schneider Electric Australia (se.com)

Schneider Electric Egypt and North East Africa