Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Z suffix on the ATV630 and ATV930 Process Drives?

Issue:

What does the Z suffix mean on the ATV630 and ATV930 Drives?

Product Line:

ATV630 and ATV930 Drives.

Environment:

The IP20 only

Cause:

Cabinet Integration versions of the ATV630...Z and ATV930...Z drives.

Resolution:

The Z suffix on the ATV630....Z and ATV930....Z are the cabinet Integration version Drives and will ship without the

-No conduit kit (size 1-5)

-No top cover

-No keypad or HMI

The drive will be IP20 rated.

ATV630 ATV930 Breakdown

Best Regards,

Gary Richardson

Schneider Electric Egypt and North East Africa