Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the minimum and maximum temperature that the metallic enclosures can withstand?

Our Spacial S3D, CRN, SBM, SF and SM enclosures and cubicles as weel as the PanelSet SFN cubicles can be used under below mentioned T°:

Conditions for use: Ambient air temperature for outdoor or indoor installations: -25 to +40 ºC.

Atmospheric conditions for outdoor installations: The humidity may temporarily reach 100% at a temperature of 25 ºC.