Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the mandatory pin assignement for DFBs in Control Expert V16.0 ?
In a DFB type, variables with mentioned types “ANY”, “ANY_INT”, “ANY_ARRAY” (and “ANY_BIT” also) can be created through the data editor. But the analyze of this DFB will fail, because such types are not supported.
The mandatory assignments of each kind of pin are the following (the other cases are optional):
    1. Inputs   => DeviceDDT, DDT-Reference, REF_TO
    2. Output => DeviceDDT, DDT-Array, anonymous array (“Array of xxx”), DDT-Reference, REF_TO
    3. Input/Output => IODDT, DeviceDDT

Schneider Electric Egypt and North East Africa