Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PME - unable to open or edit any modules in Designer, inputs/outputs are grayed out

Issue
In Designer the user is unable to open/edit any modules and inputs/outputs are grayed out.

Product Line
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment
Designer

Cause
Toolbox must be enabled and the PME user's account must have an access level of Supervisor.

Resolution 1
In Designer, go to Options > Show Toolbox
Show Toolbox in Designer

Resolution 2
If the Show Toolbox option is grayed out, ensure the user logging into Designer has an access level of Supervisor. This can be found in the PME Web Applications > Settings > Users > User Manager (also requires a Supervisor level account to view).
supervisor permission user manager

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center