How can we help you today?

Why OFS 3.63 SP3 has some start-up latency or doesn’t start?

The OFS 3.63 SP3 has integrated some CRLs access from Internet.
However, in certain condition of used, OFS can be installed on a computer where no internet connection is available.
Therefor, OFS won’t start or start with a long period of wait.
To avoid this, the proposed workaround is to bypass this step of the online CRLs access by modifying a registry key.
To do it, the value of the following registry need to be modified either using the “SetReg” tool proposed by Microsoft or manually by accessing to the registry.
  • Using SetReg by Microsoft:

The SetReg tool give the following information:
SetReg Tool 1

The parameter 3) need to be changed from TRUE to FALSE as followed by executing the following command : SetReg 3 FALSE

SetReg Tool 2
  • Modifying the registry key manually:
The involved registry key is the DWORD State key under :

KEY_CURRENT_USER\SOFTWARE\Microsoft\Windows\CurrentVersion\WinTrust\Trust Providers\Software Publishing

This is the Key registry for the current user. If your OFS is launched by a specific user, please do the same on this specific user registry key.

State valueSetReg commandEffect
0x00023e00SetReg 3 FALSEDisable CRLs online access
0x00023c00 (default)SetReg 3 TRUEEnable CRLs online access

Registry

This issue will be corrected in the next release of OFS.
  1. Product Line
OFS 3.63 SP3
  1. Environment
Windows 10, Windows Server 2022

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center