How can we help you today?

How do I rename the OFS Server default name from Schneider-Aut.OFS to a customize name?

Issue:
How to rename the OFS Server default name from Schneider-Aut.OFS to a customize name


Product Line:
OFS server


Resolution:
Renaming of the default OFS server name Schneider-Aut.OFS to a customize name must be done via the windows registry editor. To modify the name do the following:
1. Launch the windows registry editor
2. Go to  HKEY_CLASSES_ROOT\Schneider-Aut.OFS
3. Change the key name "Schneider-Aut.OFS"  to your custom name

Schneider Electric Egypt and North East Africa