How can we help you today?

How to perform a Cold Start and Dry Start on a Back-UPS unit?

Issue:
To Cold Start a Back-UPS is to kick start the unit onto battery power and to Dry Start a Back-UPS unit is to kick start the UPS on AC power.

Product Line:
Back-UPS, Back-UPS Pro, Easy UPS

Environment:
All serial numbers.

Resolution:

There are some instances that the UPS may refuse to turn on even though it is plugged into the AC outlet. It could be that the UPS does not like the power it is getting. In this case, we can apply the Cold start procedure.

To perform a Cold Start on an APC by Schneider Electric Back-UPS, you may follow the procedure below:
  1. Disconnect any attached load.
  2. Make sure the battery is connected.
  3. Unplug the UPS from the wall socket.
  4. Push and hold the ""On"" button on the UPS and let go before the second beep finishes.
  5. Plug the UPS into the wall outlet.

There are also some scenarios where the UPS is found unresponsive due to its battery charge being deeply drained and discharged and for some reason, it declines to turn on. With this being said, we can apply a Dry Start on the UPS.

To perform a Dry Start on an APC by Schneider Electric Back-UPS, you may follow the procedure below:
  1. Disconnect any attached load.
  2. Unplug the UPS from the wall socket.
  3. Disconnect the UPS' internal battery or the battery disconnect switch if any.
  4. Plug the UPS into the wall outlet
  5. Turn the UPS on.

Should there be any other questions and/or concerns, feel free to reach out to us at 1-800-800-4272 or our chat with our technical support group atAPC by Schneider Electric Customer Technical Support.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center