Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to transfer a %M using a WRITE_VAR
The following logic can be used to transfer a %M variable over Modbus TCP/IP using a WRITE_VAR block.
The BOOL_TO block is used to convert the %M type BOOL to the EMIS variable of type INT.


ghjk