Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to install Accusine PCS+ CT's for a Main-Tie-Main Installation

Issue
Example drawings for how to connect CT's for a Main-Tie-Main AccuSine PCS+ installation are not shown in the wiring diagrams in the installation guide.

Product Line
AccuSine PCS+

Resolution
Attached is an example wiring diagram showing the placement and polarity of the CT's for a Main-Tie-Main installation.  The polarity of the CT's on either side of the tie-breaker must be opposite the polarity of the CT's after the main breaker on each side.  This will allow each AccuSine to correct only the side it is installed on.

Schneider Electric Egypt and North East Africa

Attachment(s)
Example PCS+ Main-Tie-Main CT connections.pdf [343.3 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center