Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you share existing metering CT's with an AccuSine PCS+?
Issue
There may not be room in the switchgear for another set of CT's so it is possible to use an existing set CT's.  An example would be if there is a set of CT's for a power meter already installed in the gear.

Product Line
AccuSine PCS+

Resolution
Attached is an example wiring diagram showing how the existing metering CT's can be wired to the AccuSine from the power meter.  These CT's need to be wired in series to the AccuSine from the power meter.  It will not work correctly if wired in parallel.

Schneider Electric Egypt and North East Africa

Attachment(s)
PCS+ Share CT's with meter.pdf [335.61 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center