Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I download the latest Cumulative Update for PME 2021

Issue:
PME 2021 Cumulative Update

Product:
Power Monitoring Expert 2021

Environment:
Software Installation Files

Resolution:
The latest Cumulative Update (CU2) for PME 2021 and associated documentation can be found in the link below:
[PME][Download] PME 2021 Cumulative Update 2 is now released! - Schneider Electric Community

Release date: 06/2023