Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does EcoStruxure Control Expert support bit extraction of a DINT, DWORD and UDINT data type?

Issue:

Bit extraction of DINT, DWORD and UDINT data type in Ecostruxure Control Expert

Product Line:

EcoStruxure Control Expert

Resolution:

As of Control Expert V15.3, bit extraction of a DINT, DWORD and UDINT data type is allowed. Prier to this version it was not allowed.

image1

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center