Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Resolve SSH Access Issues in PowerChute Network Shutdown After Upgrading to ESXi 7.0 Update 7.0 Update 3d to 3g & from 7.0 Update 3I till 3Q?

Issue:

After upgrading to ESXi 7.0 Update 3d, SSH access might fail with one of the following symptoms:

  • If the “AcceptEnv” option is enabled in /etc/ssh/sshd_config, SSH access might fail because the SSHD process does not start, resulting in no response when connecting to the ESXi host.

Product Line:

PowerChute Network Shutdown v5.0, v5.1

Environment:

VMware vSphere ESXi 7.0.3

Solution:

Do the following steps to ensure PCNS can connect to the ESXi hosts over SSH.

  1. Log on to the ESXi host via DCUI.
  2. Execute the following command:
  3. vi /etc/ssh/sshd_config
  4. Comment out or remove the option AcceptEnv.
  5. Save and exit using the command :wq!.
  6. Restart the SSH service:
  7. /etc/init.d/SSH restart

See Broadcom support article. SSH access may fail post upgrade to ESXi 7.0 Update 3d