Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
RemoteConnect Configuration Log - Invalid Field ID

I wrote a configuration to a SCADAPack 474 while online with the controller and received the following Invalid Field errors in my Configuration Log.

This typically occurs when RemoteConnect is attempting to configure functionality that the firmware does not have.  This results in some intended functionality not being applied.

Configuration Log details below:

#Rebuilding Configuration from file configuration.rtu at 13:31:37 on 16-05-2024

File Attributes: 103799 bytes, 13:31:36 16/05/2024

File is valid. Rebuilding Configuration

# 7448: Invalid field Id: 354073

# 7496: Invalid field Id: 150901

# 7558: Invalid attribute for point: 551210

Configuration Rebuild Pass

To correct this issue apply the firmware bundled with the version of RemoteConnect that you're using.