Cannot configure the Quantum 140NOC77100 Ethernet IP module.
The Quantum 140NOC77100 Ethernet IP module can be configured in Control Expert or Unity using the attached 'Unity Pro EtherNet/IP Configuration Tool'.
The 'Control Expert' or 'Unity' software must be installed prior to the installation of the 'Unity Pro EtherNet/IP Configuration
Tool'.
'Control Expert' or 'Unity' will need to be started using 'Run as Administrator' in order to open the 'Unity Pro EtherNet/IP Configuration
Tool'.
Released for: Schneider Electric Egypt and North East Africa