How can we help you today?

VIP Sources and Data Are Slow to Populate in Web Applications

Issue

Virtual meters and other sources from the VIP are slow to come into the Web Application.

Product Line

Power Monitoring Expert 8.2

Power Monitoring Expert 9.0

Power Monitoring Expert 2020 (9.1)

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Virtual ION Processor (VIP)

Designer

Web Applications

Cause

VIP Files are meant to be less than 2 MB. Once they begin to grow past this, some performance is degraded.


Resolution

Segment out modules for multiple VIPs. Create new VIPs as needed. Reference article FA221411 for instructions on creating new VIPs.

Schneider Electric Egypt and North East Africa