Can I replace the battery inside APC Portable Power Station (Schneider OffGrid)?
Issue:
Can I replace the battery inside APC Portable Power Station (Schneider OffGrid)?
Product Line:
- Schneider OffGrid Portable Power Station models: PPS330, PPS500, and PPS730
Cause:
The APC Portable Power Station is designed to provide reliable power for your devices during outdoor activities or emergencies. Over time, the battery may fail or need to be replaced. Environmental factors impact Schneider OffGrid battery life. Elevated ambient temperatures, high humidity, poor
quality mains power causing frequent short duration discharges will shorten battery life.
Resolution:
No, the battery of APC Schneider OffGrid PPS is non-removable and not customer replaceable. If the unit requires service, please contact the APC Customer Care Center at https://www.apc.com/us/en/support/contact-us
Released for: Schneider Electric Egypt and North East Africa