Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
P1 relay I/O key(CB control key) don't work

Issue

Customer found that the I/O keys (CB control key) on P1 relay front panel doesn’t work .

_____________________________________________________________

Product Line

Power logic P1

_____________________________________________________________

Environment

2.E.22 or newer

_____________________________________________________________

Root Cause

From the version history in P1 manual, we can see that in 2.E.22 firmware, our R&D team “add enable soft-switch of the keys O/I on front-panel in menu;” and the default value is “disable”, it means when this “control keys mode” setting is “disable”, the I/O key on front panel is not working, we need to modify the “control keys mode” setting to “No confirm” or “with confirm” to use the I/O key.

_____________________________________________________________

Solution

Modify the “control keys mode” setting to “No confirm” or “with confirm” to use the I/O key on front panel.

_____________________________________________________________