Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I activate the service port mirroring of M580 CPU on the fly ?

Issue:

Can I activate the service port mirroring of M580 CPU on the fly ?

Product Line:

M580

Environment:

M580

Resolution:

User could activate the service port mirroring of M580 CPU in Control Expert ton the fly by following steps :

Online CPU DTM >>Right click CPU DTM >>Click "DTM menu" >>Click "Additional Functions " >>Click "Online action "

online DTM

Then you could select the source mirroring ports as “YES” and click update to activate the function . After that ,you could select the source port as "NO" and click update to remove the port mirroring .

Port setting