Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why the usage of Batch files ofsservice.bat and ofsnoservice.bat is not available anymore in OFS version 3.63 SP3 ?

The usage of batch files ofsservice.bat (resp. ofsnoservice.bat) may be vulnerable and are no more installed.

Solution :

Run instead regofsservice /true (resp. regofsservice /false) in a command line to register (resp. unregister) the server as a service.

Product line :

OFS 3.63 SP3

Environment :

Windows 10 and above