Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the max no. of M580 Modbus Requests that can be handled in a single/one scan cycle, and their forms ?

The below questions always cause confusion to anyone who would like to implement Modbus requests in M580 :

Presumably, if we have 3 PLCs (1, 2 & 3) that perform read and write requests using "Read_Var" & "Write_Var" blocks simultaneously. So, if we suppose that all CPUs can provide a max of 16 requests per scan on the Ethernet channel.

Accordingly :

  1. Does a request refer to the no. of implemented "Read_Var" & "Write_Var" blocks inside the the code ?. Or, does a request refer to the no. of open communication connections between each single CPU and the other 2 ones ?
  2. If the above is correct (a request refers to the communication connection between 2 CPUs), so if for example PLC1 and PLC2 are performing read and write requests between each other, will the total number of requests between them be 1 or 2 in total (a read request for the read way/route and another write request for the write way/route) ?
  3. If we consider the communication of read and write between 2 CPUs as 2 requests in total, so what is the max no. of allowable "Read_Var" & "Write_Var" blocks in a single CPU's code ?
  4. If other communication modules are present on each CPU's rack (like NOC, NOM .... etc.) which are performing read and write requests as well, so in this case will the max no. of requests for both read and write be the cumulative number of all requests performed by the present Ethernet channels (like the 16 requests presumed above) ?
  5. If NOC's DTM requests are also implemented, do they have other independent max number of requests performed, or those requests shall be considered within the max no. of the system (CPU) in total ?
  6. Finally, if the max requests no. is exceeded (>16), will there be a workaround to handle those requests per scan (like disabling a portion of them in the current scan cycle, and swapping them with the current ones in the next scan cycle simultaneously) ?

____________________________________________________________________________________________________________________________________________________________________

Based on the above questions, please consider the below :

In the implementation of a Modbus TCP communication between client and server PLCs, there are limitations related to the number of requests that can be supported in a single/one cycle, both on the client and server PLC sides. When the PLC is both in client and server modes, the maximum number of connections authorized by PLC must also be taken into account.

For the Client PLC :

Depending on the CPU reference, there is a limit on the number of requests that can be executed in one cycle in the Client PLC :

  • If it is explicit messaging, each EFs (READ_VAR, WRITE_VAR or DATA_EXCH) used in the program logic is considered as a request. As a result, there will be as many requests as EFs (READ_VAR, WRITE_VAR or DATA_EXCH) in the sections of the Control Expert PLC application
  • If it is implicit messaging, for a NOC module, each line of the ''Request settings'' tab associated with each device (Server) of the ''Device list'' of the Master DTM (DTM of the NOC in this case) is considered as a request. Similarly, for the NOE module of the M340, Premium or Quantum platform, each line of IO Scanning is considered as a request

So, max. no. of supported Modbus requests by M580 CPUs per scan cycle are :

Maximum number of requests as client per scan.PNG

For the Server PLC :

Like the client, there is a limit on the number of requests that can be processed by the PLC in server mode during a cycle. For M580, the limit on the maximum number of requests that can be handled by the PLC is split between the CPU and the communication modules (NOC).

For example, a M580 4040 can process a maximum of 32 requests in server mode during its PLC cycle. In these requests, it can only process 24 via the service port and equipment network, and the other 16 requests are received via the X bus.

The below local rack assembly example includes a BMEP584040 CPU, along two BMENOC0301/11 Ethernet communication modules. Therefore, the maximum value in this example apply to the BMEP584040 CPU (described above) :

BMEP584040 CPU and two BMENOC0301 Ethernet communication modules.PNG

When the incoming requests exceed these maximum values, they are queued in a first-in/first out (FIFO) buffer. The size of the FIFO buffer depends on the selected CPU :

  • Modbus TCP and EtherNet/IP Server: The table below shows the maximum number of Modbus TCP, EtherNet/IP, or UMAS requests that can be served by the CPU's Modbus TCP server at each MAST scan :

size of the FIFO buffer is according to the selected CPU.PNG

For the Client/Server PLC : When the PLC is both client and server at the same time, in addition to the two limitations presented above, the limitation linked to the maximum number of authorized connections must be taken into account. Below is the following table listing the maximum number of simultaneous Modbus TCP, EtherNet/IP and UMAS connections on the embedded Ethernet port, depending on the M580 CPU reference :

Number of Connections.PNG

Finally, you can refer to this FAQ < FA168406 >, to know more about Modbus, and its associated function codes

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center