Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Manage Services On The Edge Platform

Problem:

Every project within the Eclipse workspace will create its own service file in the rauc bundle. If you find multiple service files are running on your edge platform, you can delete/stop them to prevent interference.

Solution:

The unwanted services may be removed from the Edge side by deleting them, and redeploying the bundle. The default service location is as follows:

home/oecore-i686/sdk/eclipse-workspaces/default/sysroot/overlay/lib/systemd/system

Service location in VM

Alternatively, the services may be stopped and set to not start on boot via the RTU side. To do this, SSH into the Edge platform and use the following commands as necessary:

See status

systemctl status <Name>

Start/stop service

systemctl start <Name>

systemctl stop <Name>

Enable/disable autostart at boot

systemctl enable <Name>

systemctl disable <Name>

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: