Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the system requirement for EcoStruxure Control Expert v16.0 ?

System and Installation Requirements

Performance Considerations

The configuration of the computer determines the EcoStruxure Control Expert performance, which can be affected by the number of open windows, the amount of animated data that is accessed, and the size of the applications/system projects that are open.

Hardware and System Requirements

The following table describes the hardware and system requirements to install and use EcoStruxure Control Expert.

Component

Requirements

CPU

3.0 GHz or greater

Intel Core i7 or greater (or equivalent)

RAM

16 GB

Storage

20 GB free space for the software installation, execution, and for saving applications

SSD drives

Operating system

The following operating systems are supported:

  • Microsoft Windows 10, 64-bit, version 21H1 or greater
  • Microsoft Windows 10 Enterprise LTSC 2019, version 1809
  • Microsoft Windows 11, 64-bit, version 21H1 or greater
  • Microsoft Windows Server 2019 Standard, version 1809
  • Microsoft Windows Server 2022, version 21H1 or greater

Display

VGA (800 x 600) minimum resolution

Maximum supported resolution: 5120 x 1440 with Scale and Layout at 125% or greater

Input devices

Keyboard and mouse or compatible pointing device

Ports

USB port

Licenses, page 36

License activation on the Internet

NOTE: Offline activation is also possible.

Operating System Service Pack, Security Patch, and Language Requirements

Ensure that the latest Windows Service Pack and Security Patches are installed.

Ensure that the language that you select for EcoStruxure Control Expert is installed on your operating system (for example, Chinese). Otherwise, messages that are generated by the operating system use the operating system display language.

.NET Framework Installation Requirements

The following components are required before installing EcoStruxure Control Expert:

  • .NET Framework 3.5 SP1

To install .NET Framework 3.5 on supported Windows and Windows Server operating systems, either automatically or manually, ensure that the computer is connected to the Internet and that the Windows Update service is enabled.

NOTE: To download .NET 3.5 SP1, go to https://dotnet.microsoft.com/ download/dotnet-framework/net35-sp1, then click Download .NET Framework 3.5 SP1 Runtime.

  • .NET Framework 4.8

NOTE: .NET 4.8 Framework is already installed on Windows 10 version1903 and subsequent supporting versions. To download .NET 4.8 Framework, go to https://dotnet.microsoft.com/download/dotnetframework/net48 and then, click Runtime in Advanced downloads >Offline installer.

Depending on the Windows version and/or the computer configuration, .NET 3.5 SP1 can be:

  • Not installed
  • Installed but not enabled (The corresponding Windows feature is not set to ON.)
  • Installed and enabled (Only this configuration is compatible with the installation of EcoStruxure Control Expert.)

NOTE: If either .NET Framework is not installed or incorrectly configured, Setup displays a message.

Using a Virtual Machine

EcoStruxure Control Expert runs on the following virtual machines:

  • VMware Workstation Player 16 and 17
  • VMware Workstation Pro 16 and 17
  • VMware ESXi 10.0
  • Oracle VirtualBox 6.1.0

Before starting EcoStruxure Control Expert, ensure that the 3D graphics acceleration of the virtual machine is disabled. Otherwise, you may experience incorrect graphic display.

Ensure that out of the total amount of installed RAM, at least 8 GB remain available to the host computer.

Firewall

After EcoStruxure Control Expert is installed and the computer is restarted, the SE.Automation.SystemManager.Service.exe service is executed.

If a firewall is active on the computer, ensure that the execution of this service is authorized on the computer acting as Control Expert server. Otherwise, EcoStruxure Control Expert instances cannot connect to the server.