How can we help you today?

EcoStruxure Control Expert - Impossible to go in on-line mode / Error 203 message when connecting to PLC from DTM Browser

!!!Confidential Content

Issue

When in the EcoStruxure Control Expert > DTM Browser window, and attempting to Connect to the BMEP58_ECPU_EXT node via EIP Explicit communication, we get the messages:

"Impossible to go in on-line mode."

and "NA_Config Cannot StartDriver (Error 203)"

Error message dialogs

Product Line

EcoStruxure Control Expert

Cause

There are a few common causes:

A) There is a physical break in the ethernet connection

B) The IP Address Subnet of the computer is different than the PLC

C) There is a managed switch or firewall rule blocking the Ethernet/IP TCP port 44818

D) There is a separate application that is running on the computer that is reserving TCP port 44818 for itself

Resolution

Steps to troubleshoot:

For (A) physical break in the ethernet connection and (C) a managed switch or firewall rule blocking the Ethernet/IP TCP port 44818

1) Try a running a new CAT5E cable directly between your laptop/workstation running EcoStruxure Control Expert and the PLC.

2) If it works, inspect your old cable for failure, and/or inspect the settings on your managed switch to ensure passage of TCP and UDP packets on port 44818 to the PLC.

NOTE:

If the network is managed by an IT department, please contact them and tell them you would like to free up the TCP and UDP port 44818 and UDP port 2222 for Ethernet/IP communication.

For (B) IPv4 Subnet of the computer is different than the PLC

1) Go to Control Panel

2) Go to Network and Sharing Center

3) Click on "Change adapter settings"

4) Right-click and go to Properties on the Network you wish to view/edit

5) Click on "Internet Protocol Version 4 (TCP/IPv4)"

6) Change the IP Address to match the subnet of the PLC.

IP Address setting in Windows

7) Hit OK and OK again

8) In the DTM Browser screen, double-click on the PLC node (1st node directly under "Host PC")

9) In the Channel Properties, Source Address section, click on the dropdown next to IP Address Source (PC)

10) Choose the IP Address associated with the Network node of your PC

IP Address Source (PC) dropdown

11) If you needed to change this, hit [Apply] at the bottom corner.

12) Check that it matches the IP Address of the PLC from the Channel Properties > TCP/IP node:

IP Address of PLC

In the case of (D) there is a separate application that is running on the computer that is reserving TCP port 44818 for itself

1) From the Start bar search box, type "Resource Monitor"

2) Run the Windows Resource Monitor

3) Go to the Network Tab

4) Expand Listening Ports

5) Sort by the Port column

6) Find 44818

7) If the Image name is not "ControlExpert.exe", take note of what is the Image and PID of this row, this will be the software which is blocking the port.

Windows Resource Monitor - Listening Ports

For example:

If you have Rockwell Studio 5000 software installed on the same computer.

Even if Rockwell Studio is not running or RSLinx itself is not running, the process "RSLinxNG.exe" running a service called "FactoryTalk Linx OPC Runtime Service" reserves the port 44818.

One will need to stop the service from Windows Services and then ensure that the PID is indeed Terminated:

RSLinxNG.exe service

That will free up the port and allow Control Expert to use it and allow the DTM connection to the M580.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center