Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the PSP200 Portable Solar Panel work with the PPS330 Portable Power Station?

Issue:

Does the PSP200 Portable Solar Panel work with the PPS330 Portable Power Station?

Product Line:

Schneider OffGrid PSP200 & PPS330

Environment:

All serial numbers

Resolution:

The PSP200 Portable Solar Panel will work with the PPS330 Portable Power Station. However, it will limit the maximum input to 100 Watts.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: