Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
VSD in PrismaSeT I

VSD- Variable Speed Drive can be installed in PrismaSeT I Floor Standing switchboards.

Ratings starting from 0.37kW upto 110kW can be installed in IP42/54 configuration with forced cooling for an ambient ≤ 35°C.

For ambient >35°C, Type- 2 co-ordination chart can be referred.

Fan and Filter CR# with module size as per kW rating is available in EasyPrisma Software.

Note- Global door should be mandatorily plain for VSD feeders. Do Not use Glass door as you will not be able to make cut out for the fan and grills.