Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a timer in EcoStruxure Control Expert that counts up and also counts down?

Issue:
Timer in EcoStruxure Control Expert that shows the timer counting up and also counting down


Product Line:
EcoStruxure Control Expert


Resolution:
EcoStruxure Control Expert does not natively have a timer that counts down. All the standard timer blocks only count up. Attached is a DFB that shows the timer counting up and counting down.

Schneider Electric Egypt and North East Africa

Attachment(s)
TIMER_COUNT_UP_DOWN.zip [954 Bytes]