Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between EASYCAN and VARPLUS CAN Capacitor?

The difference  between Varplus Can and EasyCan is that:

EasyCAN is suitable for installations having THDi <5% and THDu of <3% while VarPlus Can is intended for installations having THDi of less than 8% and THDu of less than 5%..

For more information, you can download our Power Factor Correction catalogue on our global website via the following direct link:

https://download.schneider-electric.com/files?p_Doc_Ref=PF_Correction_2017&p_enDocType=Catalog&p_File_Name=PFCED310003EN_020617.pdf