Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Error 1720 gets returned during Control Expert install or uninstall

This can occur if the regional setting for the windows clock is incorrectly set or set to use cyrillic letters

It is recommended to ensure that the regional settings for the Windows clock on the PC' is correctly set.