Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SCADAPack 47xi - Edge Board Firmware Update

When working with SCADAPack 47xi controllers, there may come a time when a firmware update is needed. It is important to note that 47xi controllers have both RTU firmware and Edge firmware and it is important that the boards use the same version number for them to sync up properly.

Note that it is important to update the Edge firmware before the RTU firmware to help avoid synchronization issues.

Situations may arise where a customer is not using the Edge board on their 47xi and may try to update only the RTU board which could cause the boards to desync. As seen below, the Status page shows a SP474i but RemoteConnect is unable to bring back the  Edge firmware version.

SP47xi Status Page Desynced

Using a terminal program such as PuTTY, connect to Port 22 for a SSH session

Putty settings to connect to 47xi over SSH

If the Edge board root password has been forgotten, a Factory boot of the device may be required in order to assign a new Edge password with RemoteConnect.

Once logged in to the root account on the Edge board, type 'verinfo'

Verinfo results

With the Edge firmware version identified, it is possible to update the RTU firmware version to match. You may need to go into the RemoteConnect Documentation Set to find the release notes to confirm which firmware releases go together.

For example: RTU firmware 9.9.5 corresponds with Edge firmware 3.1.5

Use release notes to confirm which versions of firmware go together

Once the RTU firmware and Edge firmware are at the same level, the Edge board should sync with the RTU board and be properly reported on the RemoteConnect Status page

RTU firmware and Edge firmware versions match