Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATS480 - OCF Fault

What causes an OCF fault on the ATS480 soft starter?

Issue:

OCF fault on ATS480

Product Line:

ATS480

Environment:

All

Cause:

Excessive motor current.

Resolution:

1) Check the programming of the Soft start. Got to Menu 1.1: Motor Nominal Current- must be set to the Motor FLA.

ILT – Current limit: May need to increase to allow more current when starting. If you set too high can cause

instant OCF faults on a run command  Acc – Acceleration: May need to increase  Init Starting torque – Initial

starting torque (may not be visible depending on other settings); too high can cause OCF faults on run command.

Menu 3.5: Start and Stop: Control mode- set to Voltage Control,(some applications will respond better),

Suggest to set the boost to no.

2) Check wiring from soft start to the motor.

3) Check for blockage of the motor(ensure that the motor turns freely, if it is possible to check?)

4) Check for correct rotation of the motor.

5) Check that the motor and the soft start are sized correctly.

6) With motor connected, attempt to run motor and check the current draw on each phase of the output on the soft start.

7) If possible run motor across line and check current draw on each of the three phases (should be less than the full

load amps of the motor and should be balanced on the three phases).If the motor does not run from line power or the

current is high when running on line power, the problem is with the motor or the connected load.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center