How can we help you today?

How to configure the communication between a BMENOP0300 module and an C264 device ?

To configure a C264 device, we use the PACIS SCE tool to generate a ZIP configuration file, which is then transferred to the C264 device using another software called PACIS CAT.

It is mandatory to use this same ZIP file to configure the BMENOP0300 module, by extracting the .SCD configuration file from it and using the Modicon IEC61850 Configuration tool to transfer it to the module.

schema

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center