How can we help you today?

What is the default IP address of the Edge I/O network interface module NTSNEC1200?

Issue:

Default IP address of the Edge I/O network interface module NTSNEC1200

Product Line:

Edge I/O, NTSNEC1200

Resolution:

The default IP address of the Edge I/O NTSNEC1200 is 10.10.x.y where x.y is the last two octets of the MAC address converted to decimal.

Example:  If the MAC address is 00.80.F4.02.EA.6A then the IP address will be 10.10.234.106

EA Hex = 234 Decimal
6A Hex = 106 Decimal

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center