Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
NetBotz logging level reset to "Warning" after 5.5 upgrade

Issue:
NetBotz logging level reset to "Warning" after 5.5 upgrade

Product Line:
NetBotz

Environment:
NBRK0750
NBWL0755
Upgrade to Firmware Version 5.5

Cause:
By design, upgrading NetBotz to version 5.5 will cause logging levels to be switched to "Warning" no matter what the previous setting was.

Resolution:
Due to additional logging information that may be stored locally or be sent to a Syslog server, it was decided to set logging to warning so there would not be too much information logged.

If a different level is required, you will have to change it back to the previous setting manually after upgrade.