Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Modbus TCP Support for SCL500RM1UC and SCL500RMI1UC UPS Models

Issue: Do the SCL500RM1UC and SCL500RMI1UC UPS models support Modbus TCP?

Product Line: SCL500RM1UC and SCL500RMI1UC with SmartConnect port

Resolution:

The SCL500RM1UC and SCL500RMI1UC UPS models do not support Modbus TCP.

The User Manual of these units indicate a "Modbus TCP control" selector switch, and the switch is also present on the actual UPS. Although the switch has been retained structurally, it is not connected to the UPS circuit and is not utilized.

img

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: