Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
M251, Setting the Real Time Clock

Issue:

How do we set the real time clock (RTC) in a M251?

Product Line:

M251 controller, EcoStruxure Machine Expert

Resolution:

In the Machine Expert application, there is an example project that shows how to work with the M251 real time clock.

To access this example project, create a "New Project" and select "From Example".

Under the "General" tab, use the button with two arrows at the top right to switch from "Controllers" to "Examples" and select the "RTC Control / Timezone & Daylight Saving Time / SNTP Client - Example:"

Select the "TM251MESE" as the controller.

Give the project a name and Click the "OK" button.

Create project from Example.

See how the RTC is managed in the project.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: